相机选型工具
{{ totalBookmarksCount }}
书签收藏

The influence of temperature on image quality in SWIR cameras

新闻列表

Product News

Within the electromagnetic spectrum, infrared radiation is located between visible light and microwaves.

It covers a wide spectrum from 750 nm to 14.000 nm wavelength. It is common to separate it into near-infrared (NIR), short-wave infrared (SWIR), mid-wave infrared (MWIR), and long-wave infrared (LWIR). Although infrared radiation in the SWIR region is not visible to the human eye, it interacts with objects in a similar manner as visible wavelengths.

Most SWIR camera sensors are based on InGaAs material and work like silicon-based CCD or CMOS sensors by converting photons into electrons - so called quantum detectors. InGaAs sensors are made of Indium, Gallium, Arsenide based photodiodes and silicon-based read-out integrated circuits (ROIC). The band gap energy is typically smaller in InGaAs photodiodes than in silicon based pixels. As a result, the dark current is higher at similar temperatures.

Influence of dark current on image quality
Dark current is current that flows (for example produces a signal) even if no light is hitting the sensor. It is caused by thermal excitation of electrons in the InGaAs material. The absolute value of the dark current can vary considerably from one sensor to another. Dark current increases strongly with higher sensor temperature. As a rule of thumb, it doubles approximately every 9°C.

For example, when the same picture is taken twice with the same camera at 20°C and 45°C sensor temperature, the histograms show very different results. At 45°C sensor temperature the minimum value is higher (0 being black to 255 being white) as well as the average value. At 20°C there are no saturated pixels (max. value 254) whereas at 45°C there are quite a few.

Temperature impact on spectral sensitivity
Sensor temperature also has a high influence on the spectral sensitivity of SWIR cameras. When sensor temperature is lowered by 40°C (from 25°C to -15°C) it results in a shift of the spectral sensitivity of about 25 nm towards lower wavelengths. This might be of great importance for applications operating at the low or high end of the sensitivity curve. When sensitivity above 1.700 nm is required, sensor temperature should not be too low (which means below 20°C). Even though dark current (and noise) increase with higher temperature, the signal might still be better at the higher end of the spectrum.

Sensor temperature control is crucial
The temperature level influences the spectral sensitivity and the dark current.  The dark current has a high impact on image quality (black level and noise). For applications where image quality is important and when operating at the low or high end of the sensitivity curve, temperature control is crucial.

To accurately monitor and control the temperature, all our SWIR Goldeye cameras implement three temperature sensors:

  • inside InGaAs sensor housing
  • on sensor board
  • on mainboard

In addition, our cameras provide advanced features to correct and minimize those effects (for example advanced background correction).

To counterbalance the temperature difference between ambient and sensor temperature and to stabilize the set sensor temperature, most of the Goldeye cameras are equipped with a thermo-electric cooling device. Available cooling devices are:

  • TEC1: single-stage thermo-electric sensor cooling (for example: Goldeye G/CL-033 TEC1)
  • TEC2: dual-stage thermo-electric sensor cooling (for example: Goldeye G/CL-032 Cool TEC2)
  • Additional cooling fan (for example: Goldeye G/CL-032 Cool TEC2)

In addition, the Goldeye Cool models enclose the sensor in a Nitrogen filled cooling chamber (for example: Goldeye G/CL-008 Cool TEC1). That protects it from condensation and makes it suitable in environments where condensation is likely to occur (that is high humidity, high ambient temperatures).

Learn more about our Goldeye SWIR cameras
To learn more about the different models of our SWIR camera family and their temperature control features, please visit the Goldeye product pages on this website, or contact us today and one of our imaging experts will be happy to answer your questions.
 

Video: The influence of temperature on image quality in NIR / SWIR cameras

新闻列表