档案

Allied Vision’s 1 Product Line takes center stage at the Embedded Vision Summit 2018

Allied Vision will be exhibiting at the Embedded Vision Summit 2018 as a Premier Sponsor and showcasing the 1 product line camera platform.

Allied Vision will be exhibiting at Embedded Vision Summit 2018 in Santa Clara, California as a Premier Sponsor at the Santa Clara Convention Center from May 22-23, 2018.  Allied Vision can be found at booth #204.

 

A New Camera for Embedded Vision: The Allied Vision 1 Product Line
The Allied Vision 1 product line is a new camera platform which combines the performance of a machine vision camera with the size, power consumption and price of an embedded camera. The 1 product line gives embedded system developers and integrators access to image quality and camera performance previously unattainable for cost and space reasons.  Designed for embedded vision applications, the 1 product line is a full range of digital cameras capable of fulfilling the high standards of industrial and scientific image processing.

The heart of the 1 product line is the unique ALVIUM® technology. ALVIUM® is a proprietary chip design optimized for advanced digital imaging combined with a comprehensive image processing library (IPL) reflecting more than 25 years of expertise in industrial image processing. This shifts the image correction and optimization processing to the ALVIUM® IPL, freeing CPU capacity on the host board for alternative processing tasks.

The 130 and 140 series are the first camera families based on this platform. Both are powered by ALVIUM® technology and will be available with MIPI CSI-2 and USB3 Vision interfaces.  Furthermore, a wide range of sensors will be covered between both series.

 

Allied Vision to present at Embedded Vision Summit
Paul Maria Zalewski, Product Line Manager at Allied Vision, will be a speaker during the Embedded Vision Summit. The presentation he will give is titled, “A New Generation of Camera Modules: A Novel Approach and Its Benefits for Embedded Systems”. Attendees can listen to this presentation on Tuesday, May 22 at 1:30 pm in Exhibit Hall A-3. The presentation is part of the Enabling Technologies Summit Track. A brief synopsis can be found here.

 

Embedded Vision Summit 2018
Booth #204

May 22-23, 2018
Santa Clara Convention Center
Santa Clara, California, USA


Allied Vision Presentation
“A New Generation of Camera Modules: A Novel Approach and Its Benefits for Embedded Systems”

Tuesday, May 22, 2018 – 1:30 pm
Exhibit Hall A-3