档案

Allied Vision shows imaging solution for electronics manufacturing at Nepcon Thailand 2016

Allied Vision will showcase variety of imaging solutions for the electronics manufacturing industry at Nepcon Thailand 2016 in Bangkok on 22 – 25 June 2016.

Original image taken by camera

Scratch mark on the surface of the object

Allied Vision will be participating for the first time in Nepcon Thailand 2016, the only event for Surface Mount Technology (SMT) and electronics manufacturing industry in Thailand, from 22 – 25 June 2016 at Bangkok International Trade & Exhibition Centre (BITEC), hall 106/Booth #6C23.

Visitors can discover how Allied Vision camera technology can help them optimize their processes for quality and efficiency with two practical demos.

Barcode and OCR Inspection 

Using Mako CMOS camera for pattern recognition, this demo will showcase how vision systems can be implemented in barcode traceability and OCR verification of product code or product serialization. Mako, ultra compact affordable camera, offers simple plug and play integration into standard image processing systems.

Scratch and Contamination Inspection 

Manta G-505B will be used to demonstrate material surface inspection of small assembly part such as magnetic bracket, bolt, and screw. Allied Vision’s Manta GigE vision camera comes with a wide range of features which enable seamless integration in almost any application.

Beyond these two practical demos, Allied Vision will showcase its wide range of machine vision cameras for industrial inspection. Visitors can take the opportunity to discuss their own inspection tasks with experts from Allied Vision and its Thai partner, Dynatech Instrument

Nepcon Thailand 2016

Hall 106 / Booth #6C23

22 – 25 June 2016

Bangkok International Trade & Exhibition Centre (BITEC)