工业应用

Allied Vision’s short-wave infrared (SWIR) cameras are used in IR microscopy to detect defects during semiconductor fabrication process.

Read more

使用配备AVT Goldeye 短波红外(SWIR)相机的Axiom Optics CinCam InGaAs系统分析短波红外激光束

Read more

Highly automated production processes are usually too fast for the human eye to be able to identify the causes of errors. Allied Vision's Mako camera as part of R&D Vision's SpeedView system does not miss a single detail. The supplied images enable a precise analysis of the production process.

Read more

A number of different cameras visually support the verification of completeness and quality of the interior configuration and ambiance lighting of produced door panels.

Read more

High resolution cameras mounted in the cutter head of a tunnel boring machine enable structural analysis and geological documentation of the drilling surface.

Read more

Allied Vision 为光伏 (PV) 模块检查系统提供在量子效率和灵敏度方面表现优异的近红外 (NIR) 相机。这类产品被市场上的检查系统广泛使用,用于在弱红外线光环境下对太阳能面板进行缺陷检测和质量检查。

Read more

Following hailstorms, many vehicles must be inspected for hail damage in the shortest possible time. With the aid of 17 high-resolution Manta cameras from Allied Vision, adomea’s hail scanner MIKo quickly and thoroughly detects even the smallest dents, accelerating the claim process for insurers and vehicle owners alike.

Read more

The Spanish specialist for artificial vision, INFAIMON, has created a solution for Vision Guided Robotics that identifies, selects, picks and transfers defined objects within a bin, using Allied Vision cameras. Depending on the special requirements of the application, either the small Mako G-125 or the enhanced Prosilica GT1290 is applied.

Read more

To feed source signals into the fiber optic cable with as little loss as possible, telecommunications companies monitor lasers’ performance data using laser beam profilers equipped with infrared cameras from Allied Vision.

Read more

Predictive maintenance completed by vibration analysis is achieved with the help of Allied Vision.

Read more